Issue
Controller TAC221R is obsolete and needs to be replaced.
Environment
2212020800 Controller TAC221R
Cause
Replacement may be required since the TAC221R is obsolete since the end of 2009.
Resolution
There is no direct replacement available. In most applications, a free programmable Xenta controller with custom application is the only way to recreate functionality of the TAC 221R.