What Devices are Compatible with the SM5200 Pelco Web Viewer?

Issue

What Devices are Compatible with the SM5200 Pelco Web Viewer?

Product Line

Pelco Video Management

Environment

Endura SM5200 All Versions

Cause

Need to determine compatibility between the SM5200 and various devices.

Resolution

The table below lists the Pelco Web Viewer features available from legacy cameras, current cameras, encoders, and recorders. 

Compatibility Notes:

Current Endura Components:

  • WS5200/WS5070: Must be upgraded to version 2.5.3.10286 or later to configure operator access to the Pelco Web Viewer.
  • WS5000/WS5050/WS5060: Compatible with the SM5200 when used as a replacement for the SM5000. The user interface must be upgraded to leverage the web browser and transcoding capabilities of the SM5200.
  • VCD5202: No compatibility restrictions. When using the VCD5202 with the KBD5000 keyboard, user passwords are restricted to alphanumeric characters unless using a USB keyboard to log on.
  • WS5200- MAP: No compatibility restrictions. The Endura Mapping server installer is not required to use WS5200-MAP with the SM5200.
  • NET5402R-HD: No compatibility restrictions.

Legacy Endura Components:

  • WS5000/WS5060/WS5070: There are no compatibility restrictions when using the SM5200 as a replacement for the SM5000. You must upgrade to the WS5200/WS5070 to utilize the SM5200's remote access capabilities.
  • GW5000/NET5301TC: No compatibility restrictions. The GW5000 and NET5301TC can continue to be used for their respective functions independently of the SM5200's remote access capabilities.
  • VCD500x: User passwords must be alphanumeric unless using a USB keyboard to log on.
  • NET5301R: No compatibility restrictions.
  • NVR51xx/SEB51xx: No compatibility restrictions. Footage on NVR51xx units cannot be queried for remote search, playback, or export from the SM5200.
  • DVR53xx: No compatibility restrictions. Footage on DVR53xx cannot be queried for remote search, playback, or export from the SM5200.
  • DVR51xx: No compatibility restrictions in EnduraEnabled environments. Footage on the EnduraEnabled DVR51xx units cannot be queried for remote search, playback, or export from the SM5200.

Client Access Requirements:

  • Endura Workstation: 2.5.3.10286 or higher
  • Endura Utilities: 2.3.10.3 or higher
  • Browsers:
    • Chrome 17+
    • Firefox 8+
    • Internet Explorer 9.0+

More information on the SM5200 can be found on the spec sheet.