Changing the Automation Server HTTP / HTTPS ports

Issue

Changing the Automation Server HTTP / HTTPS ports

Product Line

SmartStruxure Solution

Environment

Automation Server version 1.3

Cause

There is a need to change the Automation Server's HTTP and / or HTTPS ports from the default ports of 80 (HTTP) and 443 (HTTPS).

Resolution

The HTTP / HTTPS ports of the Automation Server can be changed from StruxureWare Building Operation Webstation. 

  • From a web browser*, connect and log on to the Automation Server.
  • After you have logged on, click on 'Settings' near the top right corner and select 'Device Configuration'.


     
  • The TCP/IP configuration page should appear. From here, you can change the HTTP / HTTPS ports. 


     

* Supported web browsers for StruxureWare Building Operation at version 1.3 are Microsoft Internet Explorer 8 (32-bit) and 9 (32-bit), Firefox 4 or later (32-bit).

Firefox 4 or later (32-bit)