Can both an a Workstation License and an ES license be installed in the same computer?

Issue

ES will not start because only the WorkStation Software Professional license is installed and not the Enterprise Server License.

Can both licenses be installed on the same computer ?

Product Line

SmartStruxure Solution

Environment

  • Enterprise Server
  • Workstation
  • License

Cause

The enterprise server will not run because only the workstation license is installed.

Resolution

Yes both the WorkStation Software Professional license and the Enterprise Server license can be installed in the same computer.