Steps to remove I/NET Seven software and SQL database from a stand-alone PC, then install a later version of I/NET Seven

Issue

Steps to remove I/NET Seven software and SQL database from a stand-alone PC, then install a later version of I/NET Seven

Product Line

TAC I/NET

Environment

I/NET site

Cause

Need to replace existing I/NET software on a computer.

Resolution

  1. Remove I/NET Seven and MSDE; use the Add & Remove Programs utility in Windows Control Panel.
  2. Go to Windows Explorer and delete the I/NET Seven and SQL Microsoft Server folders.
  3. Go to the Icon called “My Computer” / Manager / Local Users / User / and delete the file called “INMProxy”.
  4. Empty the Windows Recycle Bin before beginning the new install.

Check compatibility by using Lessons Learned article 4240