How to setup Sarix Analytic-based Motion Detection Recording in Endura.

Issue

Using Sarix Analytics to Record specific motion-types only is different than just using generic Endura Motion Recording.

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • Pelco Endura NSM5200 Recorder all versions.
  • Pelco Endura WS5000/5200 version 2.0 or higher.
  • Pelco Sarix-based Camera and Encoder Platforms all versions.

Cause

User Requested Video Guide.

Resolution

See the following example setup procedure walkthrough.

For best viewing, press youtube Options (Gear Icon) and select 720p resolution) and full screen option at lower-right.
There is no audio, use of the pause/play while following along is recommended.