What is the part number for the DSSRV/DSSRV2 USB Recovery / Resource Key?

Issue

Would like to order the DSSRV/DSSRV2 USB Recovery/Resource Key.

Product Line

Pelco Video Management

Environment

  • DSSRV
  • DSSRV2
  • USB-DS
  • USB-DS2

Cause

Would like to recover a DSSRV/DSSRV2 back to factory defaults.

Resolution

Digital Sentry  USB Recovery Key

  • DSSRV Part Number = USB-DS (this recovery key will not work for DSSRV2) This item is obsolete.
    • See related articles for creating your own USB recovery disk.
  • DSSRV2 Part Number = USB-DS2 (this recovery key will not work for DSSRV) This is a current product.

 

The USB Key ships with the following items preloaded:

  • Recovery Image [latest release version], for DSSRV it is 7.6.32, DSSRV2 is 7.7.309
  • DS Installation Software Suite [latest release version], for DSSRV it is 7.6.32, DSSRV2 is 7.7.309
  • DS Documentation:
    • DSSRV Installation manual
    • DS ControlPoint Installation/Operation manual
    • DS Admin Operation manual

Related Articles: