Can the SM5200 Failover to the SM5000?

Issue

Can the SM5200 Failover to the SM5000?

Product Line

Pelco Video Management

Environment

  • Endura SM5000 All versions
  • Endura SM5200 All versions

Cause

  1. There is a need to configure failover on an Endura System Manager.
  2. A new SM5200 is purchased and it is desired that the old SM5000 be used as a failover.

Resolution

The SM5200 cannot failover to the SM5000 and vice versa. The SM5200 and the SM5000 are not compatible. To configure failover either two SM5000s or two SM5200s will be needed.

  • To configure failover on the SM5000 click here.
  • To configure failover on the SM5200 click here.