Issue
When logging into SIGNAL, a pop-up error appears:
Path not found. Error, Btrieve #915. A local or shared drive cannot be found. Correct the problem and try again.
Environment
SIGNAL
Cause
The SIGNAL.INI file located in the WINDOWS folder contains folder paths that no longer exist or were changed.
Resolution
Replace this file with a copy containing the default directories. The file can come from a database backup, another installation of SIGNAL, or from the link available in the previous line above.