Lock / Unlock access to Setup in DS ControlPoint.

Issue

Restricted users are still allow to access DS ControlPoint setup menu.

Product Line

Pelco Video Management

Environment

  • DS ControlPoint
    • Version 7.0.24 and above

Cause

Access permission for DS ControlPoint setup menu.

Resolution

NOTE: The Lock Setup feature locks access to shared setup options and requires a password to gain access.
 

 To lock setup: 

  1. Click on Setup
  2. Click on Lock Setup icon


     
  3. Enter a password
     
  4. Confirmed the password
     
  5. Click OK 
     
  6. Close the Setup tab 
     
  7. Go back to Setup  
     
  8. Verify the password works 


To Unlock Setup:  

  1. Click on Lock/ Unlock Setup (this will unlock the protection on the setup options).  
     
  2. Enter your password


     
  3. DS ControlPoint setup is now unlocked