How to Digital Zoom with ControlPoint?

Issue

  • Does DS ControlPoint support Digital Zoom on both Live and Playback video?
  • How to Digital Zoom with ControlPoint?

Product Line

Pelco Video Management

Environment

  • DS ControlPoint

Cause

Would like to use the Digital Zoom feature on both Live as well as Playback video.

Resolution

Yes, DS ControlPoint supports Digital Zoom on both Live and Playback video.

 

Enabling Digital Zoom:

  1. Click the Enable Digital Zoom icon
  2. Position the mouse pointer over the area of the video you want to zoom.
  3. Use the mouse wheel to zoom in and out.
  4. Click the Enable Digital Zoom icon a second time to end zooming and return to the default view.