ExSite Division rating

Issue

Division rating of ExSite is required to ensure specifications are met

Product Line

Pelco Cameras

Environment

  • IPSXM Exsite Series
  • EHXM Exsite Series

Cause

Division rating confirmation

Resolution

The Exsite Series PTZ and FIXED model are rated as follows:

  • Division I - refers to locations where the hazardous condition can exist most or all of the time. ExSite is classified to Division I standards.
  • Division 2 - refers to locations where the hazardous condition is not likely to exist under normal operating conditions. In every case, meeting Division I requirement automatically includes Division 2 compliance.

 

Click Here for the White Paper of ExSite - White Paper