How to program and recall a PTZ preset using Endura WS5000/WS5200

Issue

A PTZ preset location needs to be programmed.

Product Line

Pelco Video Management

Environment

  • WS5000 all versions
  • WS5200 all versions

Cause

A PTZ preset location is needed.

Resolution

Program a Preset:

  1. From the main workstation screen, Right click in the video pane of the desired camera. 
  2. Select Preset and then select Modify Preset.
  3. Enter the number of the preset you want to modify, and then click the OK button.
  4. The current position will be save.


Recall a Preset:

  1. From the main workstation screen, Right click in the video pane of the desired camera
  2. Select Preset
  3. Enter the number of the preset you want to activate, then click the OK button.
  4. The PTZ camera should return to the preset position previously programmed.