Predefined Preset commands when the AD-32 Preset switch is set to ON for any of the Pelco pan and tilt products.

Issue

What are the predefined preset commands when AD32 switch is ON.

Product Line

Pelco Cameras

Environment

  • Spectra II
  • Spectra III
  • Spectra IV
  • Spectra Mini
  • Esprit
  • ExSite

Cause

Predefined presets for call up.

Resolution

 Predefined Presets for AD32 Operation

If the limit stops are turned off, presets 23-26 can be used as regular presets.

The AD32 Preset Switch is featured as an option to support AD systems that do not exceed programming presets above 32.

Preset 28 allows 95 Menu access.