IWM24-GY voltage output

Issue

The IWM24-GY mount outputs higher than 24VAC power

Product Line

Pelco Cameras

Environment

  • IWM24-GY
  • IWM24-BK

Cause

Output voltage of IWM24-GY values may vary pending low or high input voltage.

Resolution

AC Output Voltage of IWM24-GY

Input                                                                        Output

102VAC                                                                  22.90 VAC

105 VAC                                                                 23.56 VAC

110 VAC                                                                 24.71 VAC

115 VAC                                                                 25.80 VAC

120 VAC                                                                 26.90 VAC

125 VAC                                                                 28.00 VAC

130 VAC                                                                 29.10 VAC

135 VAC                                                                 30.30 VAC