White or washed out video on CM6700 matrix switcher

WARNING

ELECTROSTATIC DISCHARGE REQUIRED.
Discharge all static electricity from your person by touching metal prior to handling any hardware. Failure to do so may result in damage to devices.

Issue

Individual Cameras with Video output displaying as washed/white out

Product Line

Pelco Matrix

Environment

  • CM6700 Matrix Switcher

Cause

Video Termination Settings

Resolution

CM6700 Matrix Switchers feature termination jumpers located inside the unit.

Read article LL#12686 How do I set Termination on CM6700-MXB Series Matrix Switcher