Issue
PinPoint graphics crashes when creating or editing "Active Animation" or "Combo Box"
Product Line
Andover Continuum
Environment
Windows 7 1.93 1.94
Cause
If logged on to the PC as a Power User or other non Administrator account you may not have the correct permissions to run some items within Continuum
Resolution
If the user is required to modify or create PinPoint graphics or various other activities, full access to the Continuum Folder may be required ( or Graphics Folder if this is an a remote server)
1. Log on to the PC as an Administrator
2. Locate the Continuum directory (usually C:/Program Files/Continuum) or Graphics directory
3. Open Properties (Right Click)
4. Select Security
5. Add the required Group or user name, give the write permission