How many Video/Monitor outputs does the DX8100 support?

Issue

How many Video/Monitor outputs does the DX8100 support?

Product Line

Pelco Video Management

Environment

  • DX8100 Series
  • Monitor
  • VGA
  • BNC

Cause

Would like to add as many monitors as possible to the DX8100.

Resolution

DX8100 Standard and Accessories outputs

Click here to download the full size image.

Related Articles:

How to configure the external monitor (Spot Monitor) output on the DX8100 Series HVR.

Enable the dual display card on the DX8100 Series hybrid video recorder.

Does the DX8100 come with the dual display output?