Replacement for valve V394

Issue

Since the V394 is obsolete, a proper replacement is requested.

Product Line

Field Devices

Environment

V394:

7319421000
7319425000
7319429000
7319433000
7319437000
7319441000
7319445000
7319449000

V341:

7314121000
7314125000
7314129000
7314133000
7314137000
7314141000
7314145000
7314149000

V311T:

7311717000
7311721000
7311725000
7311729000
7311733000
7311737000 
7311741000
7311745000

Cause

Replacing obsolete valve.

Resolution

Depending on application, the V311T or V341 are the closest available valves for replacement. The V341 is of Bronze material, while the V311T is Cast Iron. Depending on the valve size in question, the closest fit is the V311T, while the V341 will require pipe work. See each products data sheet for more information and details.