Can convert an ACP file to an MS Access file (MDB) (I/NET 2000)

Issue

Can convert an ACP file to an MS Access file (MDB)?

Product Line

TAC I/NET

Environment

I/NET 2000

Cause

Can convert an ACP file to an MS Access file (MDB)?

Resolution

If you are running Inet 2.xx, you have a tool to do this conversion. If you go into windows explorer\programs\Inet 2000\access-conversion editor you will see that there is a process for this. This process will allow an ACP file to convert the MDB and back to ACP files. One essential thing, if you convert the ACP file to an MDB file. DO NOT CHANGE the file structure, if you plan to convert it back to an ACP file.