StruxureWare for Building Operation Web Services Limitations

Issue

What are the limitations of Building Operation Web Services?

Product Line

SmartStruxure Solution

Environment

StruxureWare Building Operation Version 1.3

Cause

Due to the XML response rate (XML file information send to Building Operation), it has some limitations.

Resolution

General Guide in the Technical Reference Guide:

  • The limit for the whole XML response is 100 kb, which includes manually created values.
  • The limit for a string value is 10 kb, which includes manually created values.
  • The maximum number of values created in the Web Server interface is 200.
  • The recommended limit for XML elements in the Web Service interface is 100
  • The recommended number of Web Service interfaces in an Automation Server XML elements at a polling rate of 60 seconds. is 2.

Additional Information: