Issue
Do I need a CM9760-DT or a CM9760-DT-4 with my new CM9700 Matrix Switcher?
Product Line
Pelco Matrix
Environment
CM9700-CC1
CM9760-DT
CM9760-DT-4
Cause
Integrating Access Control to the CM9700 Matrix Switcher.
Resolution
The CM9700 Version 9.03.0XX software has the ability to use an Internal Data Translator on any available Sercom port on the CM9700-CC1 Version 9 and above.