Auto Generated Reports not running in 64-bit Environment

Issue

Auto Generated Reports not running in 64-bit Environment

Product Line

TAC I/NET

Environment

I/NET 2.43 64-bit

I/NET 2.42 64-bit

Cause

Issue with windows scheduler is causing Auto Generate reports to fail.

Resolution

  1. Modify existing or newly created auto generate reports.
  2. Click on the Recurrence button
  3. On the "Task" Tab, modify the "Run" string.
  4. At end of the string you will notice sch=<ScheduleName>. Add the characters"/T0" or "-T0" as shown below

Before:

 

After: