Receives Error #3 Not enough memory using DVXi recovery disks.

NOTICE

DISCONTINUED PELCO PRODUCT.
This product has been discontinued. For further information please visit pelco.com/support/discontinued-products

Issue

Using disks 3000-50953 and 3000-50954 DVXi 4.1 SR3; pop-up window error displays.

Product Line

Pelco Video Management

Environment

DVXi 4.1 SR3 recovery disk

Cause

Installation.

Resolution

A memory buffer is an area of memory used for the temporary storage of data when a program or hardware device needs an uninterrupted flow of information. Buffers are typically created in Random Access Memory (RAM) rather than on the hard disk, as fetching data from RAM is faster than retrieving it from the platter technology used in conventional hard drives.

If this error occurs during the recovery process change the RAM on the device.