Sarix Event Handler Filter

Issue

Filter START and END time frame does not trigger the programmed Handler with Source.

Product Line

Pelco Cameras

Environment

  • Spectra HD Series (5118, 5220)

Cause

Sarix event handler filter requires an NTP server to function according to filter time settings.

Resolution

Once an NTP time server is provided:

  1. Enter the Sarix System tab.
  2. For Time Settings, manually enter the IP address of the NTP server.
  3. Save settings.