Issue
Is it possible to open a time schedule from a OGC graphic when the graphic is opened from Webstation?
Environment
TAC Vista 5.1.x
Cause
In older versions of TAC Vista a "Command Point" object could be used to link to a time schedule and it worked fine in booth Webstation and Workstation. And that still works fine in Workstation but to get it to work in later versions(5.1.x) a "Dynamic Value" object must be used in the graphic editor to get it to work in Webstation.
Resolution
Use a "Dynamic value" object in the OGC editor when linking to a time schedule to get it to work in TAC Webstation.