How do I Access a Pelco PTZ Cameras' program menu using NET5400, and NET5500 Encoders?

Issue

  • Accessing a Spectra III or Spectra IV OSD (Camera Menu) from the NET5400T Web UI may be difficult to navigate to.
  • NET5500 and NET5400 PRESET 95 MENU

Product Line

Pelco Cameras, Pelco Video Management

Environment

  • NET5401T, NET5402T, NET5404T Series Encoders
  • NET5501T, NET5502T, NET5504T Series Encoders
  • Spectra Series

Cause

Feature did not exist prior to May 10, 2011.  Reference Addendum No. C4690M-A located on the NET5400T Product Page

Resolution

Software Updates may be required.  Software and documentation can be found on the NET5400T Product Page  Refer to Addendum No. C4690M-A for changes.

 
ACCESS PTZ CAMERA Program Menu (PRESET 95) 
A camera’s on-screen display (OSD) menus can be accessed directly from the Encoder Configuration tab on the Settings page.
  1. Connect to the NET5400 Series Encoder via Web Browser
  2. Login
  3. Click on Settings
  4. Click on the Encoder Configuration tab then select OSD
  5. Use the arrow keys on your keyboard to navigate through the menus then press the Enter key to make your selection

CONFIGURATION AND OPERATION FOR PRESETS AND PATTERNS
Patterns and presets can be configured directly from the OSD for third-party cameras that support these features. 
  1. Access the OSD from the Settings page as described above
  2. Using the arrow keys select Dome Settings as shown in the picture above then press the Enter Key
  3. Using the arrow keys select Presets or Patterns as shown in the picture below then press the Enter Key
  4. Proceed to program presets and patterns.  Refer to the Installation/Operation manual for the appropriate Product from Camera Solutions

 

 

 

CONFIGURATION AND OPERATION FOR PRESETS AND PATTERNS
Patterns and presets can be configured directly from the OSD for third-party cameras that support these features. Access the OSD from the Settings page of
the web application for the encoder. You can run patterns or presets from the Live View page of the web application. You must log on to the device to
configure or operate patterns and presets.

 

on your keyboard to make a menu selection.ACCESS TO CAMERA ON-SCREEN DISPLAY MENUS FROM THE ENCODER CONFIGURATION TAB
A camera’s on-screen display (OSD) menus can be accessed directly from the Encoder Configuration tab on the Settings page. You must log on to the device
before you can display OSD Configuration from the Settings page. Use the arrow keys on your keyboard to navigate through the menus. Press the Enter key
on your keyboard to make a menu selection.