Do the I/ A Series (MNL- or MNB-) controllers support more than one S-Link sensor?

Issue

Do the I/ A Series (MNL- or MNB-) controllers support more than one S-Link sensor?

Product Line

TAC I/A Series

Environment

I/A Series controllers: MNL-50, MNL-100, MNL-200, MNL-V1, MNL-V2, MNL-V3, MNL-800, MNB-V2, MNB-300, MNB-1000

S-Link sensors; MN-S1, MN-S1HT, MN-S2, MN-S2HT, MN-S3, MN-S3HT, MN-S4, MN-S4HT, MN-S5, MN-S5HT

Cause

Want to connect 2 S-LINK sensors to an I/A series controller

Resolution

No, only one S-Link sensor per controller is supported. Currently, there are no plans to add the capability of supporting a second sensor.