Issue
If not considering the design of the sensor housing, can a duct sensor function also in a room application?
Environment
Duct style sensors
Cause
A specific application is requesting this type of setup
Resolution
In general it is possible to use these sensors also for room applications. Maybe the time constant will be a little bit higher because of lower velocity which in room applications usually is irrelevant. For the SHD it might be that the sinter filter can absorb some radiant heat (if there is any).