How to install the DX8100_DX8000 Client Software.

Issue

How to install DX8100 Client software

Product Line

Pelco Video Management

Environment

  • DX8100 Client Software
  • DX8000 Client Software

Cause

Require a guide for properly DX8100 Client installation.

Resolution

  1. Verify the client PC being used meets specifications
    • Processor
      • Dual core 1.6 GHz or higher
    • Memory
      • 2 GB RAM, minimum
    • Video
      • AGP or PCI-e VGA card with minimum 64 MB video RAM (nonshared memory), 1024 x 768 or 1280 x 1024 display resolution, and DirectX(R) 8.1 API.
    • Monitor
      • SVGA or XGA with 1024 x 768 or 1280 x 1024 resolution.
    • Operating System
      • Windows 2000 (SP4) or Windows XP Professional
        DirectX 8.1 or better
        Microsoft(R) Internet Explorer(R) 6.0 and 7.0
        500 MB free disk space
         
  2. Download the latest version of DX8100_DX8000 Client
  3. Save DX8100_DX8000 Client Software to Client PC desktop.
  4. Unzip DX8100_DX8000 Client Software folder by right click and select  "Extract all"
  5. Double click DX8100_DX8000 Client Software folder.
  6. Locate DATA 1 folder and Double click on it
  7. Locate setup.exe (Application) and double click on it and follow the setup install menu.

 NOTE: DX8100 / DX8000 client requires windows administration right for the user installing the client software making changes to in the client software.

For information on downloading the latest version of DX8100 Client software, refer to article: Where can I download the DX8100 Client software?