Fixed Dome and Bullet IRV cameras with Non-Programmable DN function.

Issue

Camera Menu does not allow manual setting of Day/Night option.

Product Line

Pelco Cameras

Environment

  • FD2-IRV10-6
  • FD5-IRV10-6
  • BU5-IRV12-6
  • BU6-IRWV50-6

Cause

Entering menu of IRV Series cameras does not allow manual setting of DN change.

Resolution

IRV Series Camera is operating correctly with no malfunction. Programming change of Day/Night mode is not available. Camera operates Day/Night function automatically according to light level change.