Issue
What is the latest specification For a Continuum PC
Product Line
Andover Continuum
Environment
- Cyberstation
- SQL Server
Cause
Computer specification required.
Resolution
The PC specifications for a version does not change from the time of release, so there is no "Latest Specification" as such.
For all versions the hardware requirements are defined in the installation guide (Installation.PDF) on the software CD, or in the downloaded zip file from The Exchange Download Center for the version to be used.
This document will contain the minimum and recommended specification required for that Cyberstation version on a typical site, if any other software is to be installed on the computer or the computer is to be heavily loaded; the requirements should be increased accordingly.
The same RAM and Processor requirements will also apply to the SQL Server on a typical LAN system.
You also need to check the Software and Firmware compatibility matrix for older versions of the traditional product lines for details on the compatible operating system requirements for the version to be used.
For a V2.01 system the recommended hardware for servers and workstations are:
- Intel 8 Cores, 2 GHz or better
- 8Gb RAM
- 30Gb Available HDD space (NTFS Partition)
- CD ROM Drive
- Video resolution: 1024 x 768 pixels
- Parallel or USB port
For larger systems and where there will be a lot of Extended logging or Alarming, the Hard drive, RAM size and processor speed should be increased.