PMCL500F series monitor power supply

Issue

What is the part number for the PMCL532F monitor's power supply?

What is the part number for the PMCL524F monitor's power supply?

Product Line

Pelco Monitors

Environment

  • PMCL532F
  • PMCL524F

Cause

The ZSPPMCL532F power supplies are NOT for applications with the older PMCL500A series monitors.

Resolution

The following part numbers apply as:

  • PMCL524F monitor - ZSPPMCL524F-013
  • PMCL532F monitor - ZSPPMCL532F-014

*NOTE* - these power supplies are NOT the internal PCB level power supplies inside the monitors. These powere supplies are the external, wall plug-in power supplies.