When making changes to the Personnel Manager to show custom attribute names, are these changes seen on all Workstations or just on the Workstation where the changes are made?

Issue

When making changes to the Personnel Manager to show custom attribute names, are these changes seen on all Workstations or just on the Workstation where the changes are made?

Product Line

Andover Continuum

Environment

Continuum

Personnel Manager

Cause

Not sure if these changes will need to be made to all Workstations or if this is only required to be done once.

Resolution

Any changes to the display name of the various attributes in the Personnel Manager using the Customize Attributes setting are applied to the database and will be seen by all other Cyberstations on that network. Basically, you will only need to make these changes once and not for each Workstation in your Continuum system.