Potentiometer input on a Xenta programmable device

Issue

Can I setup a potentiometer device on a Xenta device?

Product Line

TAC Vista

Environment

Menta

Xenta 280,300 and 400

Cause

No input option is available for a potentiometer in a Xenta device

Resolution

Use a curve to create you own input lookup table.

Click here for a 10K potentiometer sample