Issue
After logging on to I/NET, an error comes up saying "Verifying Database. The database file "RptASample" has changed. Proceeding to fix up the report."
Environment
I/NET upgraded version 2.4X
Cause
The table structure that was saved with the report is different than the current database table structure.
Resolution
There is no resolution as there is nothing wrong with the report. Click on the OK button and the report will be generated. The original report's structure is different and Crystal Reports recognizes it then alters or realigns them to work in the new format.