Issue
Enabled xdriver support on the controllers with the xdriver flash file.
Comm port mode has been set to xdriver, but when the xdriver fill is attached the following error occurs.
The uprev code could not open the specified UDP file
Environment
- xdriver
- Comm port
Cause
Incorrect file path or file name used.
Resolution
Rather than typing in the xdriver file path and location, select the browse button and browse to the file location.