Is the use of Windows Server 2012 supported in release 1.3?

Issue

Is the use of Windows Server 2012 supported in release 1.3?

Product Line

SmartStruxure Solution

Environment

SmartStruxure Workstation

SmartStruxure License Administrator

SmartStruxure Device Administrator

SmartStruxure Software Administrator

SmartStruxure Enterprise Server

SmartStruxure Report Server

Cause

Many new server / PC platforms are now shipping with Windows Server 2012 pre-installed.

Resolution

SmartStruxure version 1.3 was not tested against Windows Server 2012; therefore, it is not officially supported.  Presently, Windows Server 2012 support is scheduled for release 1.5.