What are the PC requirements to run the DVR5100 remote client?

Issue

Remote view of the DVR5100 is desirable.

Product Line

Pelco Video Management

Environment

  • DVR5100 Hybrid Digital Recorder
  • DVR5100 Remote Client Software

Cause

Would like the minimum PC requirements to run the DVR5100 Remote Client Software before purchase.

Resolution

REMOTE CLIENT SPECIFICATIONS

Processor

Minimum 2.4 GHz Intel® Pentium® IV or 1.6 GHz Intel Dual-Core processor

Optimum 3.2 GHz Pentium IV

Operating System

Microsoft® Windows XP Professional SP2; Windows Vista® Business or Ultimate SP2; or

Windows 7® Professional, Ultimate, or Home Premium

Memory

Minimum 512 MB RAM Optimum 1 GB RAM

VGA Card

AGP VGA card with 128 MB RAM and DirectX® 8.1 (or later) hardware acceleration with support for 1280 x 1024 resolution monitors

Monitor

VGA monitor with a minimum 1280 x 1024 display resolution

For more information please review the DVR5100 specification.