Replacing Satchwell Sensors with Schneider Electric part numbers

Issue

Replacing Satchwell Sensors with Schneider Electric part numbers

Product Line

Field Devices

Environment

Sensors

Cause

Cross referencing older 'T' type sensors to the current version.

Resolution

Outside Sensor DOT2301 , DOT0001, DOT0002 is now STO600

Immersion Pipe Sensor DWT1701 (125mm), DWT1702 (200mm), DWT0001 is now STP660 (note, if replacing sensor only then DWA0001 required).

Strap On/Pipe Contact Sensor DST1601 , DST0001 is now STC600

Duct Sensor (mainly FCUs) DDU1803 , DDU0001 is now STD670

Duct Sensor DDT1701 (300mm) , DDT1702 (460mm) , DDT0001 is now STD660

Room Sensor DRT3453 (sensor only, no setpoint adjust) is now STR600

For other DR and DRT sensors see Lessons Learned 5213

Drayton Room Sensor A701 is now STR600D

Drayton Outside Sensor A702 is now STO600D

Drayton Immersion Sensor A703 is now STP600D

Drayton Strap On / Contact Sensor A704 is now STC600D