Do we support the DoubleTake redundancy solution with Continuum?

Issue

Do we support the DoubleTake redundancy solution with Continuum?

Product Line

Andover Continuum

Environment

Continuum

DoubleTake

Cause

This product used to be available from Andover Controls, is it still available for purchase and support today?

Resolution

The DoubleTake redundancy solution is no longer supported for use with Continuum. This third-party product (with some additional in-house custom software) has not been supported for quite some time now and there has not been any new development work done on our side of the solution (the Failover Manager I believe it was called) for over 10 years.

Marathon (AKA EverRun) is the only Disaster Recovery / Redundancy solution we currently support. Also see Lessons Learned Article #4501.