Does Continuum support Windows Server 2012?

Issue

Does Continuum support Windows Server 2012? If not, are there plans for supporting this in a future release?

Product Line

Andover Continuum

Environment

Continuum

Windows Server 2012

Windows 8

Cause

Unsure of the roadmap for support for Windows 8 and Windows Server 2012.

Resolution

The current version of Continuum (v1.94) only supports up to Microsoft Server 2008 R2 (SP1). The next release of Continuum may support MS Server 2012 if that is the OS commonly available at the time the product is qualified.

Update from Marketing.

"Today the support for Windows 8 and Windows Server 2012 is under investigation both from Technology and Market/IT adoption perspective; hence at this moment no timeline nor any commitment for its support can be provided"

This won't be addressed until the OS becomes adopted more by the general market. For details on supported Operating Systems for Continuum, consult the Compatibility Matrix link found in Lessons Learned Article #4240.