You can view live but not recorded video from Endura cameras through a UDI5000-MTRX or CM9700MDD-EVS

Issue

You can view live but not recorded video from Endura cameras via a UDI5000-MTRX or CM9700MDD-EVS.

Product Line

Pelco Video Management

Environment

UDI5000-MTRX Integration Platform., all versions
CM9760MDD-EVS Matrix Digital Decoder, all versions

Cause

The cameras have not been assigned logical numbers in the WS5000 program.

Resolution

  1. Log in to the WS5000 program.
  2. Click on Setup → Setup or press CTRL + SHIFT + S.
    FIGURE 1
    The Setup Menu
  3. Click on the Devices tab and select the cameras you wish to call up on your Matrix system.
  4. On the right-hand side, change the Camera number to match the number assigned to the camera in your PSM file, as shown in Figure 2, below.
    FIGURE 2
    Setting the camera number in the Devices tab
    For example, if the camera is referred to as "EnduraCam1105" in the PSM file, then assign the camera a number of 1105 in the setup window. Figure 3, below, shows the Endura camera number specified in a PSM file.
  5. Click on the OK button.
    FIGURE 3
    The Endura camera number in a PSM file