Properties window not displaying on points when the properties option is selected

Issue

When you select the option to view the properties of a Object nothing appears.

Product Line

TAC Vista

Environment

Vista 5.1.7

Cause

A Remote desktop session was being used at the same time as the local user was logged in.

 

 

Resolution

 

To allow the properties option to be displayed log the remote desktop user off.

The preferred option is to set the Remote desktop session to a single user session.

Here is a article that link to a single user setup.