Updating firmware and software on a RoamIO2 and Service Tool Guides

Issue

At times the firmware and software on the Roam IO2 requires updating and instructions are needed

Product Line

Andover Continuum

Environment

Roam IO2

Windows XP

Windows 7

Windows Server 2003

Windows Server 2008

Windows Mobile

Cause

Instructions for upgrading the software and firmware are provided in the User's guide, but this article places them an easy to find location

Resolution

The instructions for installing the RoamIO2 firmware and hardware are in the Bacnet Service Tool User's Guide

Download instructions for installing firmware and hardware for the RoamIO2

NOTE: Firmware can only be updated from the bacnet service tool, the Infinet service tool doesn't have the update OS option

Download RoamIO2Appl2.000002.upd firmware

Download the Bacnet Service Tool Guide + Software or Download the Infinet Service Tool Guide + Software