Video will not stream if using Pelco Media Player when closed authentication mode is selected

Issue

If using the Pelco Media player you do not get video to stream when closed authentication mode is selected

Product Line

Pelco Cameras, Pelco Video Management

Environment

Sarix cameras with closed authentication mode set and using Pelco Media player

Cause

The Pelco Media player will not stream video through the port as necessary if closed authentication is selected. The Quicktime function will work.

Resolution

In order to stream video with closed authentication use Quicktime or use Firefox.  You may use a Jpeg stream to do this in IE1.8 or 1.9