How to get the Filemaster name?

Issue

How do I get the Filemaster name?

Product Line

TAC I/NET

Environment

I/NET network

Cause

Tech support recommends you use the static IP address of the computer you will be using as a Filemaster.

Resolution

To find the IP address of a computer:

  1. Right click on Network Neighborhood and scroll down to Properties.
  2. Under the Configuration tab you will see TCP/IP, double click it.
  3. IP address will be the active tab. Within it, you will see "Specify an IP address." The top address will be your IP address.
  4. Write down this number and type it in to the Filemaster name.