Issue
Users are adding areas to a person which should be blocked by a security level.
Environment
Continuum V1.93, V1.94
Cause
Object level security is allowing the personnel profile to attach areas that should be blocked.
Users with limited access to the sites areas are having additional areas added when applying a profile.
No problems are encountered if no object level security is applied to the areas.
Resolution
This issue is resolved in V1.94 SP1 release of Cyberstation.