You cannot access an IPV6 address with Firefox through HTTPS

Issue

If using Firefox and IPV6 you cannot access an IP address if using HTTPS

Product Line

Pelco Cameras, Pelco Video Management, Pelco Transmission & Power

Environment

When using Firefox, IPV6 and HTTPS

Cause

The Firefox  program will not work with a combination of IPV6 and HTTPS

Resolution

You can use Firefox With HTTPS and IPV4, or use Chrome or IE, both will work with HTTPS and IPV6