Endura UDI5000-MTRX (MDD) Pelco and Non-Pelco Equipment Checklist

Issue

UDI5000-MTRX MDD mode equipment list requires both Pelco and Non-Pelco hardware

Product Line

Pelco Video Management, Pelco Matrix

Environment

  • Endura UDI5000-MTRX MDD Mode
  • Endura NET5402R-HD (Decoder)
  • CM9700 Matrix System Version 9

Cause

The integration between Pelco Endura 2.0 Systems and Pelco 9700 Matrix Systems require both Pelco and Non-Pelco hardware

Resolution

Pelco Hardware and Software Requirements

  1. Endura 2.0 System
  2. UDI5000-MTRX
  3. NET5402R-HD
  4. CM9700 Matrix System Version 9

Non-Pelco Hardware Requirements

  1. Ethernet to Serial Converters such as Lantronix UDS1100 or UDS2100
  2. HDMI to Composite Scalers such as Geffen GTV-HDMI-2-COMPSVIDSN
  3. BNC Female Jack to RCA Male plug adapter click here
  4. HDMI to DVI cable (Not included with the Geffin Scaler) click here

Please see LL#16380 for the MDD configuration procedure.